Gescan is your leading provider of DCC by RVE, the only solution that enables seamless installation of charging stations in any residential building, regardless of consumer demands and technical limitations. A patented electric vehicle energy management system (EVEMS) integrated into a building’s electrical infrastructure, DCC eliminates the necessity for extensive infrastructure upgrades while simplifying the process of EV charging installation. With DCC, existing service capacities are optimized, overload risks mitigated and EV chargers can connect without impacting load calculations.
When is it needed?
When you want to connect an EV charger to the feeder of a panel in an apartment or condo, where the panel of the unit is out of reach.
When you want to make a new multi-unit residential building EV ready. It’s always best to plan EV infrastructure ahead to reduce the cost of installation.
In a house/townhouse where the main panel’s capacity has been reached and you want to add an EV charger to a current installation.

Direct billing according to the energy consumed (kWh) by electric vehicles
Avoids upgrading an electrical panel that is at full capacity
No additional load on the home’s electrical panel
NEMA-3R enclosure for indoor or outdoor installation
CSA and UL listed
Real-time reading of the total panel power consumption with pre-wired current transformers (CT);
Detects when total power consumption exceeds 80% of main circuit breaker capacity and temporarily de-energizes the EV charger;
Automatically re-energizes the EV charger when the total power consumption is less than 80% of main circuit breaker capacity for more than 15 minutes.