Abbotsford

Are electric heating mats the next big thing in sustainable living?

The air you breath, the energy you choose – all of it can have an impact on your health, the environment and let’s be honest your pocketbook.  Electric floor heating is picking up in popularity amongst electricians and consumers because it’s more energy efficient and better for your health. It’s also easy to install!

Electric floor heating uses direct electric heat which means 100% of the energy input is converted to heat energy that’s used to keep you and your toes warm during the cool winter months. Because heat generated from your electric mat occurs in the floor (under your tile or hardwood) - 100% of the energy is spent on heat-generating activities only.  Whereas a ‘high efficiency’ furnace or hot water radiator has moving parts, so some of the energy is converted into something other than heat - making it 90% efficient or less.

Electric floor heating also has less air movement. Forced air circulates dust, allergens and other gross things whereas radiant heat does not. Electric floor heating is also extremely effective at heating up one area or a whole room – making it a popular replacement to baseboard heaters or hot water radiant heaters that are less effective and can be less energy efficient.  

NUHEAT has been making electric floor heating products since 1989, and their NUHEAT mats are what made the nVent NUHEAT brand famous!  Not only is it good for the environment and better for people with allergies – it’s also easy to install and cost effective. Download their brochure to learn more about NUHEAT Mats and give your feet a warm hug this winter.  


Download Now

About Electric Mats: A quick and easy to install system

Underfloor heating systems often are called low-temperature systems. Since their heating surface is much larger than other systems a much lower temperature is required to achieve the same level of heat transfer. Only 1/8’’ thick, nVent NUHEAT Custom Mats are one of the thinnest and easiest to install heating systems.  In fact, the mats can be installed in 35 minutes or less! Eliminating the need to configure the heating wires during installation, nVent NUHEAT mats are a perfect solution for renovations or additions. And because they’re extra thin, you don’t have to worry about your floor height increasing.

Pre-built like an electric blanket, the heating wires are embedded in the mat so you don’t need to configure it during installation. The custom mats come in any size and can fit any room or area.  Heat coverage is guaranteed to be consistent whether you place your mat under tile, stone, laminate or engineered wood.  It doesn’t matter how easy or complex your area or room is, they’ll match your exact dimensions.  Scroll to view all the added benefits of this system!

3 fast facts

CUSTOM MATS IN ANY SIZE AND SHAPE
They can be manufactured in only 3 days!

Custom Mats provide 100% floor coverage – without cold spots and can be manufactured in just 3 days!

Custom design your own mat for rooms with curves and angles.  

Read the data sheet to learn more about this product.

ABOUT NUHEAT CUSTOM MATS
They come with a 25 Year Total Care Warranty.

nVent NUHEAT Floor Heating Systems are covered by a 25-Year Product Warranty. The warranty covers floor heating repair or installation, floor covering installation AND the floor covering product.

Offered exclusively for installations completed by NUHEAT Certified PRO installers. Ask us about how you can get certified as an nVent NUEHAT PRO.

MORE ENERGY EFFICIENT THAN BASEBOARD HEATERS
They’re great for new construction or renovation projects.

Not only are the Mats more effective at heating up a space, they’re also more energy efficient saving your customers more money. And because they’re super thin they’re are ideal for renovation projects because they’re easy to install and won’t increase the existing floor level.

Learn how you can install this system in your new construction or renovation project.

Discover how easy it is

Custom shaped (angels and curves) NUHEAT electric floor heating mats come out of the box ready to fit the room.  Installing them is easy and can be placed in directly on to the sub floor so that tiling can begin immediately. When installing your custom matt on a laminate or engineered wood floor, a thin layer of thinset should be used.

Ready to get started? Here’s a list of materials you’ll need:

  1. Acrylic or latex modified thinset
  2. Duct tape
  3. ¼ inch square notched trowel
  4. Grouting float
  5.  Digital multimeter (ohmmeter)
  6. Thinset mixer
  7. Bucket
  8. Flat towel

Based on 50 square feet the estimated time to install this system on tile/stone floors is 25 minutes and on laminate/engineered wood floors it’s 35 minutes. Discover how easy it is to get started.

Spread modified thinset using ¼’’x

Place custom mat onto fresh thinset, press firmly to create 100% contact between the Mat, thinset and subfloor.

Secure floor sensor probe between heating wires.  

Apply a thin layer of inset and install tile/stone flooring as per manufacturer’s instructions.  

Save yourself time and money this winter


Interested in adding NUHEAT to your next project?

A cost-effective heating solution, NUHEAT electric mats are inexpensive to install and do not require ductwork or any additional equipment to operate. Both nVent NUHEAT Custom Mats and nVent NUHEAT Standard Mats offer an entirely maintenance-free heating alternative – with no cold spots.

If you’re interested in learning more, want a price quote, or just looking for a friendly chat get in touch with a Gescan specialist today. We’re always happy to help!